Note that the minimum current range (3A for model N3302A for example) describes the maximum value that can be programmed for that range. You can certainly program values that are less than the maximum value of 3A in the low range.
When the N3302A is set to the low range, the unit can operate from 0A through 3A with an accuracy of 0.1% + 5mA. When the unit is set to high range, it can operate from 0A to 30A with an accuracy of 0.1% + 10mA.
Applies to: N3300A, N3301A, N3302A, N3303A, N3304A, N3305A, N3306A, N3307A
Visit our Power Products Forum for additional topics and discussions. Read technical postings on our Power Blog – Watt’s Up? |